:RSOurce:CONNect:GPIB:ADDRess
Flex Apps:
FlexPLL
Command Syntax
:RSOurce:CONNect:GPIB:ADDRess <address>
<address> is an integer.
Query Syntax
:RSOurce:CONNect:GPIB:ADDRess?
Description
Enters a FlexPLL's source instrument's GPIB address for connecting via GPIB. Use the :RSOurce:CONNect:METHod command to specify a GPIB connection. The address can be any integer from 0 to 30. The default value is 7. Use the :RSOurce:CONNect:GPIB:INAMe command to specify name of the GPIB interface.