:RSOurce:CONNect:VLAN:INDEX
Flex Apps:
FlexPLL
Command Syntax
:RSOurce:CONNect:VLAN:INDEX <device index>
<device index> is an integer from 0 to 15.
Query Syntax
:RSOurce:CONNect:VLAN:INDEX?
Description
Enters a VLAN Device Index for the FlexPLL's source instrument for connecting via the VLAN LAN protocol. The Device Index is and integer with a default value of 1. Use the :RSOurce:CONNect:METHod command to specify a LAN connection. Use the :RSOurce:CONNect:LSERver command to select the VLAN (VXI-11) LAN protocol.