:RSOurce:CONNect:STATe?
Flex Apps:
FlexPLL
Query Syntax
:RSOurce:CONNEct:STATe?
Query Response
{CONN | NCON | TOUT}
Description
Queries the state of the connection between FlexPLL and an FlexPLL's source instrument. To connect to the source, use the :RSOurce:CONNect command. To disconnect, use the :RSOurce:DISConnect command. Returns one of the following strings:
CONN- A connection is established to FlexPLL's source instrument.
NCON- A connection is not established.
TOUT- A connection to FlexPLL's source instrument has timed out.