:RSOurce:CONNect:HLAN:PORT
Flex Apps:
FlexPLL
Command Syntax
:RSOurce:CONNect:HLAN:PORT <port number>
<port number> is an integer from 0 to 65535.
Query Syntax
:RSOurce:CONNect:HLAN:PORT?
Description
Enters a HLAN HiSLIP Device Port for a DCA-X for connecting via the HLAN LAN protocol. The port number can range from 0 to 65535 with the default value of 4880. Use the :RSOurce:CONNect:HLAN:INDEX command to specify HiSLIP Device Index for the connection. Use the :RSOurce:CONNect:METHod command to specify a LAN connection. Use the :RSOurce:CONNect:LSERver command to select the HiSLIP LAN protocol.