:RSOurce:CONNect:LSERver
Flex Apps:
FlexPLL
Command Syntax
:RSOurce:CONNect:LSERver {VLAN | HLAN | SOCKets
Query Syntax
:RSOurce:CONNect:LSERver?
Description
When connecting FlexPLL to an FlexPLL's source instrument via LAN, you can selects the type of LAN server used to make the connection. The following three protocols are available:
- VLAN (default setting)
- Selects a Virtual Local Area Network (VLAN). This is the VXI-11 selection for LAN Server in FlexPLL's Source Setup dialog. Use this command to configure the server:
- HLAN
- Selects a High Speed Local Area Network (HLAN). This is the HiSLIP selection for LAN Server in FlexPLL's Source Setup dialog. Use these commands to configure the server:
- SOCKets
- Selects sockets (Ethernet Port). This is the Sockets selection for LAN Server in FlexPLL's Source Setup dialog. Use this command to configure the server: