:RSOurce:CONNect:GPIB:INAMe
Flex Apps:
FlexPLL
Command Syntax
:RSOurce:CONNect:GPIB:INAMe "interface name"
"interface name" is a string. This command supports the DEFault common child command.
Query Syntax
:RSOurce:CONNect:GPIB:INAMe?
Description
Enters the name of the GPIB interface for connecting to the FlexPLL's source instrument via GPIB. Use the :RSOurce:CONNect:GPIB:ADDRess command to specify the GPIB address. Use the :RSOurce:CONNect:METHod command to specify a GPIB connection.
Example Command Sequence
:RSOurce:CONNect:GPIB:INAMe "gpib3"