:RSOurce:CONNect:HLAN:INDEX
Flex Apps:
FlexPLL
Command Syntax
:RSOurce:CONNect:HLAN:INDEX <device index>
<device index> is an integer from 0 to 15.
Query Syntax
:RSOurce:CONNect:HLAN:INDEX?
Description
Enters a HLAN HiSLIP Device Index for the FlexPLL's source instrument for connecting via the HiSLIP LAN protocol. The Device Index can be any integer from 0 to 15 with the default value of 0. Use the :RSOurce:CONNect:HLAN:PORT command to specify the HiSLIP Port number for the connection. Use the :RSOurce:CONNect:METHod command to specify a LAN connection. Use the :RSOurce:CONNect:LSERver command to select the HiSLIP LAN protocol.