:RSOurce:CONNect:HOST
Flex Apps:
FlexPLL
Command Syntax
:RSOurce:CONNect:HOST "hostname"
"hostname" is a string. This command supports the DEFault common child command.
Description
Sets or queries the FlexPLL's source instrument's host name when connecting via a LAN. Use the :RSOurce:CONNect:METHod command to specify a LAN connection. Use the :RSOurce:CONNect command to make the actual connection.