:RSOurce Subsystem
Flex Apps:
FlexPLL
Use the :RSOurce (Remote Source) subsystem commands to connect FlexPLL's source instrument to FlexPLL. These commands configure the FlexPLL application's Remote Source fields in the Source Setup dialog. To configure the Jitter fields in the same dialog, use the commands in the :JSOurce subsystem.
- Use
:RSOurce:CONNectto connect to the source instrument. - Use
:RSOurce:CONNect:METHodto select the type of connection: LAN, USB, or GPIB. The remaining commands in the:RSOurce:CONNectSCPI node are used to define or query the selected connection type. - Use
:RSOurce:CONNect:STATequery to determine if a connection is established to the FlexPLL's source instrument. - Use
:RSOurce:DISConnectto break a connection to the source instrument.