:RSOurce:CONNect:SOCKets:PORT
Flex Apps:
FlexPLL
Command Syntax
:RSOurce:CONNect:SOCKets:PORT <port number>
<port number> is an integer from 0 to 65535.
Query Syntax
:RSOurce:CONNect:SOCKets:PORT?
Description
Enters the Sockets Port number for the FlexPLL's source instrument for connecting via the sockets LAN protocol. The port number is an integer with a default value of 5025. Use the :RSOurce:CONNect:METHod command to specify a LAN connection. Use the :RSOurce:CONNect:LSERver command to select the Sockets LAN protocol.