This section lists the test equipment needed to run performance tests and adjustments, any critical specification requirements, and recommended model numbers. The computer and all test equipment are connected to the device under test (DUT) using GPIB.
|
|
In all test equipment configurations, cables and adapters must be properly torqued. Exceeding recommended torque values can cause damage to a cable or adapter, and can cause inaccurate test results. |
|
|
|
|
Test Equipment |
Recommended Models |
Alternate Models |
Applicable Tests/Comments |
|
Analyzers |
|||
|
N9030B Options: 5xx1, MPB2, Pxx3, and N9063EM0E Analog Demodulation Measurement application4, 5
|
N9030A Options: 5xx1, MPB2, Pxx3, and N9063EM0E Analog Demodulation Measurement application4, 5, 6 E444xA7, 8, 9 Options: [11010 or 1DS10], 12311, 23312
|
Phase Modulation Deviation Accuracy |
|
|
Vector Signal Analyzer1
|
89441A Opt AYA, AYH, AY9, B7A, UFG |
|
|
|
Vector Signal Analysis Application Required for the N9030A/B. |
89600 VSA with these options:
NOTES:
|
|
|
|
Audio Analyzer1
|
8903B Opt 011 or 0511
|
|
|
|
8902A |
Phase Modulation Frequency Response |
|
|
Sources |
|||
|
External Baseband |
N5182B Option 656 or 657 |
N5182A Opt 651, 652, or 654 E4438C Opt 001, 002, 601, or 602 |
Used only in Digital Mod Power Level Accuracy Relative to CW test if UUT does not have Baseband Generator. |
|
Function Generator |
33622A |
33611A 33250A |
|
|
Reference Source (The reference source must have a frequency high enough based on the test points being tested. Note that test points are not the same as the frequency range of the DUT. Therefore, some alternative models may not be sufficient for all DUTs. The E8257D recommended model is sufficient for all DUT configurations.) |
E8257D Opt UNR, UNX, or UNY
|
8664A Opt 004 |
|
|
Meters and Sensors |
|||
|
Power Meter |
N1914B |
N1914A1 E4418A
|
|
|
Power Sensor (See below for calibration service ordering guidelines.) |
N8482A |
N8482A CFT
|
|
|
Digital Voltmeter |
3458A Opt 002 |
34470A1
|
|
|
Other Devices |
|||
|
Mixer1
|
0955-2225 |
M/A COM MDC-164 |
|
|
Mixer1
|
0955-2225 |
M/A COM MDC-174 M/A COM MDC-1641
|
|
|
20 GHz Mixer1
|
0955-2225 |
0955-1017 |
|
|
Local Oscillator1
|
E8267D Opt UNR, UNX,or UNY |
E4428C Opt [503 or 506] E8241A Opt UNJ E8247C Opt UNR E8257D Opt UNR or UNX or UNY N5181B/82B Opt [503 or 506] and Opt [UNX or UNY] |
Comments: E4428C Opt 503 is used only with ESGs with Opt 502 or 503; Opt UNJ is only required for Digital Modulation Quality test. E4438C Opt 502 is used only with ESGs with Opt 502; Opt 503 is for ESGs with Opt 502 or 503; Opt 504 is for ESGs with Opt 502, 503, or 504. E44x8C Opt UNB is not required, but typical output power is usually insufficient without it installed. E82xxx Opts UNJ, UNR, and UNX are only required for Digital Modulation Quality test. E8663B Option UNW is not disallowed, but typical output power is usually insufficient with it installed. N5181B/82B Options UNX and UNY are only required for Digital Modulation Quality test. E8663D Options UNX and UNY are only required for Digital Modulation Quality test. |
|
Frequency Standard |
10 MHz house standard. |
|
Used for Adjustments |
|
Frequency Counter |
53230A Opt [106 or 115] |
53132A Opt 050 or 124 |
|
|
Phase Noise System
|
N5511A Options 540, CH21
|
E5505A |
|
To use the PXA N9030A with N9063EM0E analog demodulation measurement application functionality above 3.5 GHz, the N9030A must be upgraded with one of the following upgrade options: MTU or TES. After either upgrade, the N9030A must be re-calibrated for analog demodulation specifications above 3.5 GHz to be valid.
Choose from one of the following options:
Option MTU — Multi-Touch User Interface
For analog demodulation specifications above 3.5 GHz to be valid, Option MTU can only be installed on N9030A instruments with serial number prefix greater than or equal to MY/SG/US5449.
Option TES — TOI Enhanced Specifications
Option TES is a Keysight-only internal option. Keysight service centers need to contact the CSG support node to obtain an internal license key for this option.
USB power sensors require a power meter with USB ports. The table below shows the various options that will provide USB ports on the N1914A power meter. Note that the recommended power meter model N1914B comes standard with USB ports.
|
N1914A Orderable Options |
Description |
FW responds as option1 |
|
|
201 |
Ordered from the factory with new N1914A |
Dual channel average power meter with VGA, trigger in/out, 1 front and 1 rear USB port |
008, 010, 012 |
|
The following options are ordered as upgrades to an existing N1914A power meter. |
|||
|
106 |
This is the recommended option. |
Dual channel average power meter with 1 front and 1 rear USB port |
008 |
|
103 |
alternate |
Dual channel average power meter, battery, 2 rear USB ports |
001, 009 |
|
105 |
alternate |
Dual channel average power meter with VGA, battery, 1 front and 1 rear USB port |
008, 010 |
|
108 |
alternate |
Parallel rear-panel sensor input connectors, front-panel reference calibrator connector, 2 rear USB ports |
002, 009 |
|
109 |
alternate |
Parallel rear-panel sensor input connectors, rear-panel reference calibrator connector, 2 rear USB ports |
003, 009 |
|
111 |
alternate |
Dual channel average power meter, battery, 1 front and 1 rear USB port |
001, 008 |
|
167 |
alternate |
Dual channel average power meter, external trigger in/out, 1 front and 1 rear USB port |
008, 012 |
|
Use the following guidelines to ensure power sensors used by the N7800A application receive the correct calibration service:
Order Option 1A7 when ordering new power sensors that will be used as working standards in N7800A TME calibrations.
When ordering periodic calibration for instruments used as lab standards in the N7800A software, we recommend using “Keysight Cal + Uncertainties + Guardbanding”. More information can be found at http://www.keysight.com/find/americas_cal.
The N7800A software incorporates the ISO GUM Uncertainty in point-to-point uncertainty calculations. The special “H-series” calibration options (shown on the Special Calibrations Matrix located at http://cal.software.keysight.com) provide lower measurement uncertainties through use of direct comparison to devices directly characterized by NPL or NIST (or another NMI). The overall resulting N7800A measurement uncertainties then reflects these lower device uncertainties. The equipment requirements of each N7800A calibration application are summarized in the Special Calibrations Matrix which can be found at http://cal.software.keysight.com.
Option H99 is a special option for the Roseville Service Center [only] which provides electronic calibration data available as a .csv file that can be imported into TME thus avoiding manual entry. Option H99 must be requested from the Roseville Service Center upon re-calibration only of any previously purchased power sensor and not for new purchases of power sensors. This option may be ordered in addition to any other required or requested Std Lab Calibration option. Option H99 is recommended but not required.
|
|
The following models are not supported by Option H99:
|