:CALibrate:CONNection:ENABled

Command Syntax

:CALibrate:CONNectionN:ENABled {ENABled | DISabled}

Where N identifies a specific instrument by connection number and must be selected from {1:8}. For an instrument that occupies multiple connections, use the instrument's left-most connection number to identify the instrument. For two-connection instruments, the connection number would be 1 or 3. For four-connection instruments, the connection number would be 1.

Query Syntax

:CALibrate:CONNection{1:8}:ENABled?

Description

For the indicated connection number, selects or deselects all listed calibrations. The listed calibrations vary depending on the type of instrument installed.

The command query indicates if all calibrations are enabled or disabled or partially enabled.

To set the availability of individual calibrations, use the :CALibrate:CONNection:VERTical command.

To perform all selected calibrations, use the :CALibrate:CONNection:STARt command.

ENABled
Selects all calibrations for the indicated connection number to be performed.
DISabled
Prevents all calibrations for the indicated connection number from being performed.

Query Response

{ENAB | DIS | PART}
ENAB
Indicates that all calibrations for the indicated connection number are selected.
DIS
Indicates that all calibrations for the indicated connection number are disabled.
PART
Indicates that some calibrations for the indicated connection number are selected and some are deselected.