:CALibrate:CONNection:SKEW:STATus?

Query Syntax

:CALibrate:CONNectionN:SKEW:STATus?

Where N identifies a specific instrument by connection number and must be selected from {1:8}.

Description

Queries the Skew Adjustment status for the indicated connection number.

One of the following response strings is returned:

"CALIBRATED"
The calibrations are valid.
"UNCALIBRATED"
At least one calibration is needed.
""
An empty string is returned if the hardware for the indicated connection number does not exist. An -241,"Hardware missing" error is returned by the :SYSTem:ERRor:NEXT? command.

Use the child queries listed in the following table to return details about the current calibration.

Status String Child Queries
Status String Child Query to Send
Time of last adjustment,
Time change since last adjustment, and
Temperature change since last adjustment
:CALibrate:CONNection:SKEW:STATus:DETails?
Change in temperature :CALibrate:CONNection:SKEW:STATus:DTEMperature?
Change in Time :CALibrate:CONNection:SKEW:STATus:TIME?

Child Commands