:CALibrate:CONNection:SKEW:STATus:TIME?
Query Syntax
:CALibrate:CONNectionN:SKEW:STATus:TIME?
Where N identifies a specific instrument by connection number and must be selected from {1:8}.
Description
For the indicated connection number, determines the oldest date and time between the last Skew Adjustment and returns the value.
If an adjustment has not yet been performed, an empty string is returned.