:CALibrate:CONNection:VERTical:STATus?

Query Syntax

:CALibrate:CONNectionN:VERTical:STATus?

Where N identifies a specific instrument by connection number and must be selected from {1:8}. For an instrument that occupies multiple connections, use the instrument's left-most connection number to identify the instrument. For two-connection instruments, the connection number would be 1 or 3. For four-connection instruments, the connection number would be 1.

Description

Queries the calibration status of a vertical calibration in the indicated connection number. One of the following response strings is returned:

"CALIBRATED"
The calibration is valid.
"UNCALIBRATED"
The calibration is needed.
""
An empty string is returned if the hardware for the indicated connection number does not exist. An -241,"Hardware missing" error is returned by the :SYSTem:ERRor:NEXT? command.

Use the child queries listed in the following table to return details about the current calibration.

Status String Child Queries
Status String Child Query to Send
Time of last calibration,
Time change since last calibration, and
Temperature change since last calibration
:CALibrate:CONNection:VERTical:STATus:DETails?
Change in temperature :CALibrate:CONNection:VERTical:STATus:DTEMperature?
Change in Time :CALibrate:CONNection:VERTical:STATus:TIME?

Child Commands

Parent Command