Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:CALibrate:CONNection:SKEW:STATus:DTEMperature?

:CALibrate Connection Commands
  • :CALibrate:CONNection:CLOCk
  • :CALibrate:CONNection:ENABled
  • :CALibrate:CONNection:EXPort
  • :CALibrate:CONNection:IMPort
  • :CALibrate:CONNection:SKEW:ENABled
  • :CALibrate:CONNection:SKEW:STATus?
  • :CALibrate:CONNection:SKEW:STATus:DETails?
  • :CALibrate:CONNection:SKEW:STATus:DTEMperature?
  • :CALibrate:CONNection:SKEW:STATus:TIME?
  • :CALibrate:CONNection:STARt
  • :CALibrate:CONNection:STATus?
  • :CALibrate:CONNection:STATus:DETails?
  • :CALibrate:CONNection:STATus:DTEMperature?
  • :CALibrate:CONNection:STATus:TIME?
  • :CALibrate:CONNection:TIMebase:ENABled
  • :CALibrate:CONNection:TIMebase:EXPort
  • :CALibrate:CONNection:TIMebase:IMPort
  • :CALibrate:CONNection:TIMebase:STARt
  • :CALibrate:CONNection:TRIGger:ENABled
  • :CALibrate:CONNection:VERTical
  • :CALibrate:CONNection:VERTical:STATus?
  • :CALibrate:CONNection:VERTical:STATus:DETails?
  • :CALibrate:CONNection:VERTical:STATus:DTEMperature?
  • :CALibrate:CONNection:VERTical:STATus:TIME?

Query Syntax

:CALibrate:CONNectionN:SKEW:STATus:DTEMperature?

Where N identifies a specific instrument by connection number and must be selected from {1:8}.

Description

Queries the change in the instrument's temperature from the time when the last Skew Adjustment was performed on the indicated connection number.

If an adjustment has not yet been performed, a value of NaA (9.91E+37) is returned.

An adjustment should be performed if the change in temperature exceeds ±5°C.

Parent Command

  • :CALibrate:CONNection:SKEW:STATus?