:CALibrate:CONNection:SKEW:ENABled
Command Syntax
:CALibrate:CONNectionN:SKEW:ENABled {ENABled | DISabled}
Where N identifies a specific instrument by connection number and must be selected from {1:8}.
Query Syntax
:CALibrate:CONNection{1:8}:SKEW:ENABled?
Description
This command enables or disables Skew Adjustment as part of the oscilloscope's Frame Adjustment procedure.
Query Response
{ENAB | DIS}