:CALibrate:CONNection:VERTical:STATus:TIME?

Query Syntax

:CALibrate:CONNectionN:VERTical:STATus:TIME?

Where N identifies a specific instrument by connection number and must be selected from {1:8}. For an instrument that occupies multiple connections, use the instrument's left-most connection number to identify the instrument. For two-connection instruments, the connection number would be 1 or 3. For four-connection instruments, the connection number would be 1.

Description

Queries the date and time of the last vertical calibration for the indicated connection number. If a calibration has not yet been performed, an empty string is returned.

Example Returned Status String

"09/20/2012 15:11:05"

Parent Command