:CALibrate:CONNection:VERTical:STATus:DETails?
Query Syntax
:CALibrate:CONNectionN:VERTical:STATus:DETails?
Where N identifies a specific instrument by connection number and must be selected from {1:8}. For an instrument that occupies multiple connections, use the instrument's left-most connection number to identify the instrument. For two-connection instruments, the connection number would be 1 or 3. For four-connection instruments, the connection number would be 1.
Description
Queries a string of status details for the current vertical calibrations for the indicated connection number (instrument). The following is an example of a typical returned string:
Time of last Calibration: 10/23/2012 11:52:00,Elapsed Calibration Time: 3 hours 2 minutes,Temperature Change: 1.24 C"
If a calibration is recommended, the following shows an example of the returned string:
"Elapsed cal time has exceeded 10 hours.,Connection 1 Channel 1 Vertical Calibration is recommended; it will be included in the Channel 2A Vertical Calibration.,Time of last Calibration: 09/20/2012 15:11:05,Elapsed Calibration Time: 27 days,Temperature Change: 2.83 C"
If a calibration has not yet been performed, the following string is returned:
"This calibration has never been performed in this instrument."
Example Returned Status String
"Requires Clock Recovery Calibration,Time of last Calibration: 03/14/2012 11:52:00,Elapsed Calibration Time: 75 hours 2 minutes,Temperature Change: 3.40 C"
Example Returned Status String
"Time of last Calibration: 03/22/2012 14:52:00,Elapsed Calibration Time: 55 minutes,Temperature Change: 0.20 C"