:CALibrate:CONNection:VERTical:STATus:DTEMperature?

Query Syntax

:CALibrate:CONNectionN:VERTical:STATus:DTEMperature?

Where N identifies a specific instrument by connection number and must be selected from {1:8}. For an instrument that occupies multiple connections, use the instrument's left-most connection number to identify the instrument. For two-connection instruments, the connection number would be 1 or 3. For four-connection instruments, the connection number would be 1.

Description

Queries the change in the oscilloscope's temperature from the time when the last vertical calibration was performed on the indicated connection number. If a calibration has not yet been performed, a value of NaA (9.91E+37) is returned. A calibration should be performed if the change in oscilloscope temperature exceeds ±5°C. Use the :CALibrate:CONNection:VERTical command to enable a vertical calibration.

Example Returned Status

2.830000000E+00

Parent Command