:CALibrate:CONNection:VERTical

Command Syntax

:CALibrate:CONNectionN:VERTical {ENABled | DISabled}

Where N identifies a specific instrument by connection number and must be selected from {1:8}. For an instrument that occupies multiple connections, use the instrument's left-most connection number to identify the instrument. For two-connection instruments, the connection number would be 1 or 3. For four-connection instruments, the connection number would be 1.

Query Syntax

:CALibrate:CONNection{1:8}:VERTical?

Description

For the indicated connection number (instrument), enables or disables the vertical calibration. To perform this calibration along with all other selected calibrations for the indicated connection number, use the :CALibrate:CONNection:STARt command. To select all calibrations for the indicated connection number, use the :CALibrate:CONNection:ENABled command. These commands affect the Calibration dialog box indicators.

ENABled
Selects the calibration.
DISabled
Prevents the calibration.

Use the child queries listed in the following table to return details about the current calibration.

Status String Child Queries
Status String Child Query to Send
State of Calibration :CALibrate:CONNection:VERTical:STATus?
Time of last calibration,
Time change since last calibration, and
Temperature change since last calibration
:CALibrate:CONNection:VERTical:STATus:DETails?
Change in temperature :CALibrate:CONNection:VERTical:STATus:DTEMperature?
Change in Time :CALibrate:CONNection:VERTical:STATus:TIME?

Query Response

{ENAB | DIS | PART}
ENAB
Indicates that all vertical calibrations for the indicated connection number are selected.
DIS
Indicates that all vertical calibrations for the indicated connection number are disabled.
PART
Indicates that some vertical calibrations for the indicated connection number are selected and some are deselected.

Child Commands