:CALibrate:CONNection:STATus:TIME?

Query Syntax

:CALibrate:CONNectionN:STATus:TIME?

Where N identifies a specific instrument by connection number and must be selected from {1:8}. For an instrument that occupies multiple connections, use the instrument's left-most connection number to identify the instrument. For two-connection instruments, the connection number would be 1 or 3. For four-connection instruments, the connection number would be 1.

Description

For the indicated connection number, determines the oldest date and time between the last vertical calibration, precision timebase, or clock recovery calibrations and returns the value. If a calibration has not yet been performed, an empty string is returned.

Example Returned Status String

"03/22/2012 14:52:00"

Parent Command