:CGMemory:TBASe:RFALl:METHod
Command Syntax
:CGMemoryN:TBASe:RFALl:METHod {AUTO | ABSolute}
Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.
Query Syntax
:CGMemoryN:TBASe:RFALl:METHod?
Description
For the indicated color grade memory, selects the method used to define the waveform top and base definitions. The command is equivalent to setting the signal's Top-Base Definition in the Thresholds > Rise/Fall tab of the Configure Measurements dialog box.
- AUTO
- Specifies that the top (100%) and base (0%) levels be automatically determined using a histogram of the signal's amplitude values. This is the default setting.
- ABSolute
- Allows you to enter absolute values for the top-base levels. When
ABSoluteis selected, use the:CGMemory:THReshold:RFALl:TOPand:CGMemory:THReshold:RFALl:BASEcommands to enter the signal's top and base levels.
Example Command Sequence
:CGMemory1:THReshold:RFALl:TRACking OFF :CGMemory1:TBASe:RFALl:METHod ABSolute :CGMemory1:THReshold:RFALl:BASE -125E-3 :CGMemory1:THReshold:RFALl:TOP 125E-3