:CGMemory:THReshold:GENeral:PMIDdle

Command Syntax

:CGMemoryN:THReshold:GENeral:PMIDdle  <percent>

Where <percent> is a decimal number from -25.0 to +125.0.

Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.

Query Syntax

:CGMemoryN:THReshold:GENeral:PMIDdle?

Description

When the threshold method is a custom PERCent between top and base (see :CGMemory:THReshold:GENeral:METHod), the :CGMemory:THReshold:GENeral:PMIDdle command sets or queries the custom middle percent value.

Example Command Sequence

:CGMemory2:THReshold:GENeral:TRACking OFF
:CGMemory2:THReshold:GENeral:METHod PERCent
:CGMemory2:THReshold:GENeral:PUPPer 125E-3
:CGMemory2:THReshold:GENeral:PMIDdle 0E0
:CGMemory2:THReshold:GENeral:PLOWer -125E-3