:CGMemory:THReshold:RFALl:PUPPer
Command Syntax
:CGMemoryN:THReshold:RFALl:PUPPer <percent>
<percent> is a decimal number from -25.0 to +125.0.
Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.
Query Syntax
:CGMemoryN:THReshold:RFALl:PUPPer?
Description
When the threshold method is a custom PERCent between top and base (see :CGMemory:THReshold:RFALl:METHod), the :CGMemory:THReshold:RFALl:PUPPer command sets or queries the custom upper percent value.
Example Command Sequence
:CGMemory2:THReshold:RFALl:TRACking OFF :CGMemory2:THReshold:RFALl:METHod PERCent :CGMemory2:THReshold:RFALl:PUPPer 125E-3 :CGMemory2:THReshold:RFALl:PLOWer -125E-3