:CGMemory:THReshold:GENeral:UPPer

Command Syntax

:CGMemoryN:THReshold:GENeral:UPPer <amplitude>

<amplitude> is a double.

Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.

Query Syntax

:CGMemoryN:THReshold:GENeral:UPPer?

Description

Sets or queries the General threshold's upper threshold-definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :CGMemory:THReshold:GENeral:PUPPer command.

Use the :CGMemory:THReshold:GENeral:METHod command to set waveform threshold levels to standard percentages or custom definitions.

Use the :CGMemory:THReshold:GENeral:MIDDle command to enter a middle threshold level. Use the :CGMemory:THReshold:GENeral:LOWer command to enter a lower threshold level.

Example Command Sequence

:CGMemory2:THReshold:GENeral:TRACking OFF
:CGMemory2:THReshold:GENeral:METHod ABSolute
:CGMemory2:THReshold:GENeral:UPPer 125E-3
:CGMemory2:THReshold:GENeral:MIDDle 0E0
:CGMemory2:THReshold:GENeral:LOWer -125E-3