:CGMemory:THReshold:GENeral:MIDDle
Command Syntax
:CGMemoryN:THReshold:GENeral:MIDDle <amplitude>
<amplitude> is a double.
Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.
Query Syntax
:CGMemoryN:THReshold:GENeral:MIDDle?
Description
Sets or queries the middle threshold-definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :CGMemory:THReshold:GENeral:PMIDdle command.
Use the :CGMemory:THReshold:GENeral:METHod command to set waveform threshold levels to standard percentages or custom definitions.
Use the :CGMemory:THReshold:GENeral:UPPer command to enter a upper threshold level. Use the :CGMemory:THReshold:GENeral:LOWer command to enter a lower threshold level.
Example Command Sequence
:CGMemory6:THReshold:GENeral:TRACking OFF :CGMemory6:THReshold:GENeral:METHod ABSolute :CGMemory6:THReshold:GENeral:UPPer 125E-3 :CGMemory6:THReshold:GENeral:MIDDle 0E0 :CGMemory6:THReshold:GENeral:LOWer -125E-3