:CGMemory:THReshold:GENeral:HYSTeresis
Command Syntax
:CGMemoryN:THReshold:GENeral:HYSTeresis <plus_or_minus_value>
<plus_or_minus_value> is a double.
Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.
Query Syntax
:CGMemoryN:THReshold:GENeral:HYSTeresis?
Description
When the :CGMemory:THReshold:GENeral:METHod setting is HYSTeresis, this command sets the user-defined ±hysteresis value for the waveform source.
Use the :CGMemory:THReshold:GENeral:MIDDle command to enter the center threshold level.
Example Command Sequence
:CGMemory2:THReshold:GENeral:TRACking OFF :CGMemory2:THReshold:GENeral:METHod HYSTeresis :CGMemory2:THReshold:GENeral:HYSTeresis 125E-3 :CGMemory2:THReshold:GENeral:MIDDle 0E0