:CGMemory:THReshold:RFALl:LOWer

Command Syntax

:CGMemoryN:THReshold:RFALl:LOWer <amplitude>

<amplitude> is a double.

Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.

Query Syntax

:CGMemoryN:THReshold:RFALl:LOWer?

Description

Sets or queries the Rise/Fall threshold's lower threshold-definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :CGMemory:THReshold:RFALl:PLOWer command.

Use the :CGMemory:THReshold:RFALl:METHod command to set waveform threshold levels to standard percentages or custom definitions.

Use the :CGMemory:THReshold:RFALl:UPPer command to enter a upper threshold level.

Example Command Sequence

:CGMemory3:THReshold:RFALl:TRACking OFF
:CGMemory3:THReshold:RFALl:METHod ABSolute
:CGMemory3:THReshold:RFALl:UPPer 125E-3
:CGMemory3:THReshold:RFALl:LOWer -125E-3