:CGMemory:THReshold:GENeral:TRACking
Command Syntax
:CGMemoryN:THReshold:GENeral:TRACking {{ON | 1} | {OFF | 0}}
Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.
Query Syntax
:CGMemoryN:THReshold:GENeral:TRACking?
Query Response
{1 | 0}
Description
Specifies whether a signal tracks the global threshold definition or uses its own threshold definition.
The global threshold definition is set using the :MEASure:THReshold:GENeral commands (see Threshold Configuration Commands).
Example Command Sequence
:CGMemory2:THReshold:GENeral:TRACking OFF :CGMemory2:THReshold:GENeral:METHod ABSolute :CGMemory2:THReshold:GENeral:UPPer 125E-3 :CGMemory2:THReshold:GENeral:MIDDle 0E0 :CGMemory2:THReshold:GENeral:LOWer -125E-3