:CGMemory:THReshold:GENeral:PUPPer

Command Syntax

:CGMemoryN:THReshold:GENeral:PUPPer  <percent>

<percent> is a decimal number from -25.0 to +125.0.

Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.

Query Syntax

:CGMemoryN:THReshold:GENeral:PUPPer?

Description

When the threshold method is a custom PERCent between top and base (see :CGMemory:THReshold:GENeral:METHod), the :CGMemory:THReshold:GENeral:PUPPer command sets or queries the custom upper percent value.

Example Command Sequence

:CGMemory2:THReshold:GENeral:TRACking OFF
:CGMemory2:THReshold:GENeral:METHod PERCent
:CGMemory2:THReshold:GENeral:PUPPer 125E-3
:CGMemory2:THReshold:GENeral:PMIDdle 0E0
:CGMemory2:THReshold:GENeral:PLOWer -125E-3