:CGMemory:THReshold:GENeral:AUTO
Command Syntax
:CGMemoryN:THReshold:GENeral:AUTO
Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.
Description
When you select the ± Hysteresis threshold definition for the selected signal (see :CGMemory:THReshold:GENeral:METHod), you can send :CGMemory:THReshold:GENeral:AUTO to automatically set the Center Threshold (:CGMemory:THReshold:GENeral:MIDDle) to be halfway between Vmin and Vmax and the Hysteresis value (:CGMemory:THReshold:GENeral:HYSTeresis) to be ±0.05(Vmax - Vmin).