:CGMemory:THReshold:GENeral:STZero
Command Syntax
:CGMemoryN:THReshold:GENeral:STZero {{ON | 1} | {OFF | 0}}
Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.
Query Syntax
:CGMemoryN:THReshold:GENeral:STZero?
Query Response
{1 | 0}
Description
When you select the ± Hysteresis threshold definition for the selected signal (see :CGMemory:THReshold:GENeral:METHod), you can turn ON the :CGMemory:THReshold:GENeral:STZero setting to move thresholds within ±10 mV to zero. This feature is useful for differential signals.