:CHANnel:PROBe:REMove:ATTenuation

Command Syntax

:CHANnelN:PROBe:REMove:ATTenuation <attenuation>

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

<attenuation> is a double.

Query Syntax

:CHANnelN:PROBe:REMove:ATTenuation?

Description

In the probe deembedding RemoveCable/Probe correction mode, when Limit Boosting corrected bandwidth is selected (see :CHANnel:PROBe:REMove:CBANdwidth), this command lets you control the attenuation applied to the signal. You can select a limit from 1.14:1 to 3.98:1. The default attenuation is 2.000:1. Lower attenuations can give you faster signal rise times but can also mean higher noise.

The same adjustment in terms of gain can me made using the :CHANnel:PROBe:REMove:DECibels command.