:CHANnel:PROBe:REMove:DELay
Command Syntax
:CHANnelN:PROBe:REMove:DELay {OFF | ON}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:PROBe:REMove:DELay?
Query Response
{0 | 1}
Description
In the probe deembedding RemoveCable/Probe correction mode (see :CHANnel:PROBe:CORRection:MODE), this command lets you enable or disable applying the delay imposed by the model to the waveform. When enabled, the waveform is accurately shifted in time according to the model.