:CHANnel:PROBe:REMove:GRAPh:IMPMagnitude
Command Syntax
:CHANnelN:PROBe:REMove:GRAPh:IMPMagnitude {OFF | ON}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:PROBe:REMove:GRAPh:IMPMagnitude?
Query Response
{0 | 1}
Description
When Probe AC Response Correction graphs are shown (see :CHANnel:PROBe:REMove:GRAPh:SHOW), this command enables or disables the Input Impedance Magnitude graph.