:CHANnel:PROBe:REMove:BANDwidth
Command Syntax
:CHANnelN:PROBe:REMove:BANDwidth <Hz_value>
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
<Hz_value> is a double.
Query Syntax
:CHANnelN:PROBe:REMove:BANDwidth?
Description
In the probe deembedding RemoveCable/Probe correction mode (see :CHANnel:PROBe:CORRection:MODE), when Specify Bandwidth corrected bandwidth is selected (see :CHANnel:PROBe:REMove:CBANdwidth), this command lets you specify the bandwidth limit of a filter to remove unwanted high-frequency noise.