:CHANnel:PROBe:REMove:GRAPh:MGRaph

Command Syntax

:CHANnelN:PROBe:REMove:GRAPh:MGRaph {FRMagnitude | FRPHase | IMPMagnitude
   | IMPPhase | FMAGnitude | FPHase}

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:PROBe:REMove:GRAPh:MGRaph?

Description

This command selects the AC Response Correction graph that should be maximized in the graph display area when using the :CHANnel:PROBe:REMove:GRAPh:DMAXimized command:

  • FRMagnitude — Frequency Response Magnitude
  • FRPHase — Frequency Response Phase
  • IMPMagnitude — Input Impedance Magnitude (Probe AC Response Corrections only)
  • IMPPhase — Input Impedance Phase (Probe AC Response Corrections only)
  • FMAGnitude — Filter FR Magnitude
  • FPHase — Filter FR Phase