:CHANnel:PROBe:REMove:PROBe
Command Syntax
:CHANnelN:PROBe:REMove:PROBe
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Description
In the probe deembedding RemoveCable/Probe correction mode (see :CHANnel:PROBe:CORRection:MODE), when probe calibrations are selected (see :CHANnel:PROBe:REMove:TYPE), this command launches the RemoveProbe AC calibration wizard.
Use the :REMove Subsystem commands to control the wizard progression.