:CHANnel:PROBe:REMove:GRAPh:SHOW
Command Syntax
:CHANnelN:PROBe:REMove:GRAPh:SHOW {OFF | ON}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:PROBe:REMove:GRAPh:SHOW?
Query Response
{0 | 1}
Description
In the probe deembedding RemoveCable/Probe correction mode (see :CHANnel:PROBe:CORRection:MODE), when cable/probe AC response calibration corrections are loaded, either by running the RemoveCable or RemoveProbe wizards (see :CHANnel:PROBe:REMove:CABLe or :CHANnel:PROBe:REMove:PROBe) or by loading a previously calibrated corrections file (see :CHANnel:PROBe:REMove:FILe), this command enables or disables the graphical user interface's Show Graphs option. When enabled, you can view the correction and analysis graphs in a graphical user interface content window.