:CHANnel:PROBe:REMove:DECibels
Command Syntax
:CHANnelN:PROBe:REMove:DECibels <dB_value>
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
<dB_value> is a double.
Query Syntax
:CHANnelN:PROBe:REMove:DECibels?
Description
In the probe deembedding RemoveCable/Probe correction mode, when Limit Boosting corrected bandwidth is selected (see :CHANnel:PROBe:REMove:CBANdwidth), this command lets you control the maximum amount of gain applied to the signal. You can select a limit from 1.14 dB to 12 dB. The default limit is 6 dB. Higher gains can give you faster signal rise times but can also mean higher noise.
The same adjustment in terms of attenuation can me made using the :CHANnel:PROBe:REMove:ATTenuation command.