:CHANnel:PROBe:REMove:CABLe

Command Syntax

:CHANnelN:PROBe:REMove:CABLe

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Description

In the probe deembedding RemoveCable/Probe correction mode (see :CHANnel:PROBe:CORRection:MODE), when cable calibrations are selected (see :CHANnel:PROBe:REMove:TYPE), this command launches the RemoveCable AC calibration wizard.

Use the :REMove Subsystem commands to control the wizard progression.