:CHANnel:PROBe:REMove:NFILe

Command Syntax

:CHANnelN:PROBe:REMove:NFILe <quoted_string>

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

<quoted_string> is a ...

Query Syntax

:CHANnelN:PROBe:REMove:NFILe?

Query Response

<quoted_string>

Description

In the probe deembedding RemoveCable/Probe correction mode (see :CHANnel:PROBe:CORRection:MODE), for differential SMA probes only, this command lets you load a previously calibrated negative-side hardware corrections file.

Use the :CHANnel:PROBe:REMove:CFILe command to load the combined (pos+neg averaged) corrections file.