:CMODe:CRECovery:CEIDle

Command Syntax

:CMODeN:CRECovery:CEIDle {ON | OFF | 1 | 0}

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

Query Syntax

:CMODeN:CRECovery:CEIDle?

Description

Enables or disables the Contains Electrical Idle option.

When you are decoding a serial bus that has bursts of serial data followed by long periods of idle time, enabling the Contains Electrical Idle control will remove idle time from the decoded serial data.

To specify the Idle Clock Count, use :CMODe:CRECovery:ICCount.