:CMODe:CRECovery:PLL:STIMe

Command Syntax

:CMODeN:CRECovery:PLL:STIMe <settling_time>

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

<settling_time> is a double.

Query Syntax

:CMODeN:CRECovery:PLL:STIMe?

Description

Specifies the settling time as a number of time constants. All PLLs take a finite amount of time to lock on to their source signal. During this settling time portion of the acquisition record, jitter measurements, protocol decode, etc. will not be performed.

Example Command Sequence

:CMODe1:CRECovery:MODE FOPLl
:CMODe1:CRECovery:PLL:STIMe 5.0