:CMODe:CRECovery:ECLock:EDIRection

Command Syntax

:CMODeN:CRECovery:ECLock:EDIRection {RISing | FALLing | BOTH}

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

Query Syntax

:CMODeN:CRECovery:ECLock:EDIRection?

Description

Specifies the edge(s) used in the explicit clock.

Example Command Sequence

:CMODe1:CRECovery:MODE ECLock
:CMODe1:CRECovery:ECLock:EDIRection BOTH