:CMODe:CRECovery:CSKew

Command Syntax

:CMODeN:CRECovery:CSKew <seconds>

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

<seconds> is a double.

Query Syntax

:CMODeN:CRECovery:CSKew?

Description

For PAM type signals (see the :CMODe:SIGNal:TYPE command), this command can be used to center the eye opening at the clock locations by shifting the clocks relative to the data.