:CMODe:CRECovery:SRATe:STATus:DETails?
Query Syntax
:CMODeN:CRECovery:SRATe:STATus:DETails?
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
Query Response
Refer to the table "Common Reasons for INV or QUES Status".
Description
If the status of the clock recovery symbol rate is questionable or invalid (see :CMODe:CRECovery:SRATe:STATus?), this query returns a string that may provide additional details.
If the status of the clock recovery symbol rate is valid, this query returns an empty string.
For a basic reason for the questionable or invalid status, use the :CMODe:CRECovery:SRATe:STATus:REASon? sibling query.