:CMODe:CRECovery:PRESets:SELections?
:CMODe CRECovery Commands
- :CMODe CRECovery Commands
- :CMODe:CRECovery:CEALgorithm
- :CMODe:CRECovery:CEIDle
- :CMODe:CRECovery:CFRequency:EDIRection
- :CMODe:CRECovery:CFRequency:MODE
- :CMODe:CRECovery:CSKew
- :CMODe:CRECovery:CSRate?
- :CMODe:CRECovery:DDRFive:CAFLatency
- :CMODe:CRECovery:DDRFive:CAFSource
- :CMODe:CRECovery:DDRFive:DQSSource
- :CMODe:CRECovery:DDRFive:POLength
- :CMODe:CRECovery:DDRFive:PRLength
- :CMODe:CRECovery:DDRFive:RWMode
- :CMODe:CRECovery:DDRFive:STDDelay
- :CMODe:CRECovery:DREMoval
- :CMODe:CRECovery:ECLock:ALIGn
- :CMODe:CRECovery:ECLock:CFRequency
- :CMODe:CRECovery:ECLock:CMULtiplier
- :CMODe:CRECovery:ECLock:DELay
- :CMODe:CRECovery:ECLock:EDIRection
- :CMODe:CRECovery:ECLock:SOURce
- :CMODe:CRECovery:FOPLl:LBANdwidth
- :CMODe:CRECovery:FOPLl:LBDivisor
- :CMODe:CRECovery:FSRate
- :CMODe:CRECovery:ICCount
- :CMODe:CRECovery:MODE
- :CMODe:CRECovery:PLL:EDIRection
- :CMODe:CRECovery:PLL:MODE
- :CMODe:CRECovery:PLL:SSCCorrect
- :CMODe:CRECovery:PLL:SSPercent
- :CMODe:CRECovery:PLL:SSType
- :CMODe:CRECovery:PLL:STIMe
- :CMODe:CRECovery:PLL:TDEPendent
- :CMODe:CRECovery:PRESets
- :CMODe:CRECovery:PRESets:SELections?
- :CMODe:CRECovery:SOPLl:JTF:LBANdwidth
- :CMODe:CRECovery:SOPLl:JTF:LBDivisor
- :CMODe:CRECovery:SOPLl:JTF:PEAKing
- :CMODe:CRECovery:SOPLl:OJTF:DFACtor
- :CMODe:CRECovery:SOPLl:OJTF:LBANdwidth
- :CMODe:CRECovery:SOPLl:OJTF:LBDivisor
- :CMODe:CRECovery:SRATe
- :CMODe:CRECovery:SRATe:STATus?
- :CMODe:CRECovery:SRATe:STATus:DETails?
- :CMODe:CRECovery:SRATe:STATus:REASon?
- :CMODe:CRECovery:TOPLl:DFACtor
- :CMODe:CRECovery:TOPLl:NFReq
- :CMODe:CRECovery:TOPLl:PFReq
- :CMODe:CRECovery:TRACking
- :CMODe:CRECovery:ZOPLl:LFPole
- :CMODe:CRECovery:ZOPLl:PPOLe
- :CMODe:CRECovery:ZOPLl:SPOLe
Query Syntax
:CMODeN:CRECovery:PRESets:SELections?
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
Description
Returns the available presets as a quoted string of comma-separated preset names.
You can select one of the presets using the :CMODe:CRECovery:PRESets command.