:CMODe:CRECovery:ECLock:DELay
Command Syntax
:CMODeN:CRECovery:ECLock:DELay <seconds>
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
<seconds> is a real number time value in seconds.
Query Syntax
:CMODeN:CRECovery:ECLock:DELay?
Description
When an Explicit clock recovery method is selected (see :CMODe:CRECovery:MODE), this command specifies a delay that is added to each of the clock times. For example, entering 1 ps will add 1 ps to each of the clocks recovered from the explicit clock source.